LTE TDD
Generates a waveform based on your current configuration. This function also checks for waveform errors prior to playing the waveform.
This function applies to Waveform Playback capability only.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:GENerate |
SCPI Example |
:RAD:LTET:WAV:GEN |
Notes |
Set only (Action) It is an overlapped SCPI |
State Saved |
No |
Preset |
When the user presets the instrument, generation operation will be canceled. |
Initial S/W Revision |
A.14.00 |
Sets the state of real-time waveform playing.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe[:STATe] OFF|ON|0|1 [:SOURce]:RADio:LTETdd:WAVeform:RTIMe[:STATe]? |
SCPI Example |
RAD:LTET:WAV:RTIM ON RAD:LTET:WAV:RTIM? |
State Saved |
No |
Preset |
When the user presets the instrument, generation operation will be canceled. |
Initial S/W Revision |
A.14.00 |
Remote command only.
Stops waveform generation.
For a real-time carrier, this command affects the generation of a real-time carrier. When the generation of a real-time carrier is stopped, the state of real-time stays on OFF. The state of real-time is not changed when this command is sent during the state of real-time is ON.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:STOP |
SCPI Example |
:RAD:LTET:WAV:STOP |
Notes |
Set only (Action) |
State Saved |
No |
Initial S/W Revision |
A.14.00 |